Hi there,
First post - be gentle! I recently purchased a RTK Express kit, upgraded to new firmware and done some test logging over some sites (trig pillars in the UK) to check accuracy with PPP post processing.
One issue I had was when starting up the satellites were zero, and a vertical fill like bar (see attached image). I changed SD cards, powered off and on numerous times, then just went through all the modes (rover/base/bubble and so on) until it decided to reset and sort itself out. Can anyone explain why this is happening and how to get around it quicker?
For serial output I used a USB C to USB C cable to my laptop from the Ublox port and can read the NMEA fine as a COM port at 9600. However, when I use bluetooth I get a virtual COM port and when connected (using PuTTY) get a semi garbled message (looks like a binary packet, then the ASCII NMEA). Is there any way I can resolve this so that I can use the bluetooth connection on a PC?
Connecting to my phone using SW maps and the bluetooth connection is fine…
The only other issue I have is when PPP processing using the TOP106 antenna. Most online services have a pull down menu where you select what antenna you have (and this one is not on the list). I also note, that some services comment that there is no antenna info within the RINEX data itself. Is there a way to add this info into a file header or similar?
Any help would be much appreciated.