RTK Config will connect, but I am not able to get on rtk.local to make any changes or update any keys.
Try going to the IP address 192.168.4.1
I am having the same issue with not being able to connect to rtk.local when my device is in Config mode. I tried going to the IP address, but that doesn’t work either.
Have you tried holding the power button for 10 seconds to attempt a soft reset?
Sometimes if it gets stuck in a loop it can help to connect to a PC over serial to trigger a reset (or firmware update if needed…I would only recommend this if the above doesn’t work)