RTK FACET NTRIP SERVER

hello,

I’m a beginner in this topic, I would like to connect my rtk drone to the rtk facet, via ntrip server, but as far as I understand I should guarantee an internet connection perhaps via hotspot or sim module to be able to connect and send corrections via caster rtk2go or emlid, my question is then, is it possible to connect rtk facet to hotspot or does it need a module to connect. someone already has experience in this field, any advice or experience would be of great help to me.

Daniel

It has WiFi and BLE - you can send correction info over either one of those

Run through the hookup guide here https://learn.sparkfun.com/tutorials/2188 which covers most of the basics

Hello,

Thanks for the reply, if i can i will post the second questions I have here:

I would need some information for the RTK FACET, the first I would like to know if the updates that I find in github are the same for all rtk products, that is, if the update for rtk surveyor is also good for the facet? The other question is, once i’ve insert the survey in for base station mode, with ntrip server, the facet starts with base mode but does not go to survey and and therefore does not create the data transmission, I miss some steps or I have to act on the RTK FACET, thanking you in advance, best regards , Daniel.