I would like to feed RTCM data via Bluetooth to the Rover from my Phone. I can do this with the switches set in the default positions. I also need to supply my Tractor Autosteer system with NMEA Data via RS232 and I have the necessary max 232 wired to the proper connector. If I slide the Serial 1 NMEA connector to EXT Cntr I can get Data out the Data port but I can no longer use Bluetooth for RTCM data. I can send RTCM data thru the Radio port via rs232/max232 and get a RTK lock. Can I tap into that UART with the two holes above the word serial or is there something I missed?
Related topics
| Topic | Replies | Views | Activity | |
|---|---|---|---|---|
| RTK Surveyor: no output on Bluetooth serial or data UART | 10 | 912 | January 27, 2023 | |
| RTK Surveyor no NMEA over data port | 3 | 1757 | May 5, 2023 | |
| Simultaneous Bluetooth and USB output from RTK surveyor | 4 | 1385 | September 19, 2023 | |
| RTK SURVEYOR WON'T STREAM NMEA OVER BLUETOOTH | 1 | 921 | July 27, 2022 | |
| RTK Surveyor - Need dual output (BT & NMEA RS232 @38400 baud) | 18 | 1781 | October 1, 2024 |