SEN-14066 ME6 Nano Simultaneous RFID reader with SPX-15113 and WRL-18071 UHF RFID Ring Antennas

Please, the SEN-14066 ME6 Nano Simultaneous RFID reader can be used with SPX-15113 or WRL-18071 UHF RFID Ring Antennas to read WRL-14147 UHF RFID Tags? If yes, the SPX-15113 or WRL-18071 can be better than the internal antenna?

The internal antenna will be better for tags WRL-14147 and WRL-14151.

The ring antennas WRL-15113 and WRL-18071 are only required for tags KIT-16464 and won’t work well for the other tags.

I am designing an application that I have to read TAGs at a 90-degree angle and a distance of 30 cm. The internal antenna is not working well for this application. I believe that an external antenna little better than the internal one can work. So which antenna, such as 60mm ceramic, can be used with this reader?

[Our external antenna will work with the M6E, there’s also a list of other antennas that work with the M6E in our [hookup guide.

Reading tags at an angle can be tricky and will result in lower read ranges. You might want to check the video below for more information on the different things that affect read range.

https://www.youtube.com/watch?v=rSbSYp2hexs](https://learn.sparkfun.com/tutorials/simultaneous-rfid-tag-reader-hookup-guide/all)](https://www.sparkfun.com/products/14131)