SparkFun GPS-RTK-SMA Base Kit

Hello I have some agricultural land to measure. I would like to know if apart from the SparkFun GPS-RTK-SMA Base Kit which would be the best option for the rover. I have 3 rasperry pi 4 in stock that I could have as a complement to your sparkfun gnns-rtk cards. My question is whether to measure polygons with a precision of 14mm the rover must be the same card as the base station? SparkFun GPS-RTK-SMA Kit or can i buy : 1.- SparkFun GPS-RTK Dead Reckoning ZED-F9R Connection Guide EITHER 2.- SparkFun GPS-RTK Dead Reckoning pHAT for Raspberry Pi, taking advantage of the fact that I have some raspberry pi 4 available. Can the SparkFun GPS-RTK Dead Reckoning pHAT be used as a rover to measure polygons with an accuracy of 14 mm without being installed in a car or without being installed in a drone? I would like to install it in my drone in the future, for now only as a rover for the base station. Thank you for your prompt response, explanation and recommendation. Thank you very much.

Please note the ZED-F9R cannot be operated in base mode. You will need a ZED-F9P for that. The GPS-RTK-SMA uses the ZED-F9P.

My question is whether to measure polygons with a precision of 14mm the rover must be the same card as the base station?

In general, any two RTK products can be mixed and matched. You should be fine using the pHAT with any other ZED-F9x product we sell.

Can the SparkFun GPS-RTK Dead Reckoning pHAT be used as a rover to measure polygons with an accuracy of 14 mm without being installed in a car or without being installed in a drone?

Yes. The ‘Dead Reckoning’ bit really only applies to vehicles when:

  • Wheel ticks are provided to the board and

  • GNSS signal goes away (like when the car enters a tunnel)

If you’re walking, driving, even flying, around a field, with a clear view of the sky, the ZED-F9R (dead reckoning version) will perform identically to the ZED-F9P in terms of accuracy.