Trying to find stepper cable connector

I’m looking to find a replacement for a stepper cable that got damaged. The connector in question seems to be some kind of JST or Molex thing with 11 positions.

The pitch of the connector seems to be about 2.5 mm, and it has these locking/polarizing keys on it. The stepper motor is NEMA 23, and the connector also has 11 positions, but only 6 are filled (4 for the two coils, and 2 for what I assume is ground).

I took some photos, they are attached.

Connector on cable/wire side:

and on the stepper motor:

Based on these, would [this housing (Digikey no. 455-2216-ND) be appropriate for this set of connectors as a replacement? What sort of connector could it be to begin with?](XHP-11 JST Sales America Inc. | Connectors, Interconnects | DigiKey)