I’d like to change the default behavior of the Trigger Settings via the WTConfig app from Robertsonics (disable re-trigger). I can see how the Trigger Numbers in the app (1-16) relate to the pins on the board but how can this be set for i2c? Is there a method to have different trigger settings via i2c like there is with discreet trigger pins? If not, which trigger does the i2c connection use as a default?
https://learn.sparkfun.com/tutorials/ts … nd-example Just download the library @ link and follow along ![]()