Hello, I purchased a WIG-18159 Tsunami Super WAV Trigger and I can not play any sounds.
If there is no SD-Card inside, the LED blinks blue, when I hold the user button und press the reset button.
The same with any Card (including update file) is 1 long blink, followed by 2 short blinks: Hex file error.
Power on with a USB-C Loader and Card inside, there is no blinking LED. Should be one time blinking, for Card is not readable or 3 times for ok.
I´ve tried with 4 different SD-Cards from 128mB up to 32GB. Formatted with FAT32 and also FAT16.
What can I do now or is the WAV-Trigger defekt?