Hi,
I just received a WIG-18159 Tsunami Super WAV Trigger and it seems not to work correctly or I can`t get it to work.
As first step I downloaded the qwiic tsunami demo mono files, placed them on a freshly deleted and formatted sd card
but pulling triggers to ground didn`t do anything, no sound and no visual feedback from leds.
I then tried with stereo files, but also no sound and no leds lighting up.
I then downloaded the firmware, and tried to update the firmware, I followed instructions on the user guide and when
trying to update with this new firmware I get visual feedback from the led:
One long blink two short blinks, which in the manual is called as „Hex file error“.
I tried updating both mono and stereo firmwares, but both result in the same „One long blink two short blinks“.
I tried with two sd cards with same results (both work in my older wavtrigger boards).
I found another thread here and also followed the suggestions there, I measured 3V3 Volt with power via usb and via a 5V
power supply, in both cases I can measure 3.3 Volts, the usb socket however seems a bit „wonky“.
When pushing buttons user and reset with no sd card inserted I get a blue light blinking.
Now I`m out of ideas. Is something wrong with the board or am I overseeing something?
I´d be really helpful for any hints or suggestions.