I am a bit confused about which Iridium module is available in ALC. Is it the plain rock7 module, or the (much improved I understand after discussing with some other people: available as I2C so does not eat a serial, better way to charge the supercapacitors, etc) Sparkfun iridium module similar to:
I would like to be able in ALC to use the “much improved” iridium module . But it seems based on communication requirements (serial) that we only get the “plain rock7” at the moment.
Ok, that confirms the first message. The thing is if I need to build a “supporting” plate on which to fix components, and then to use a qwiick cable instead of having stuff soldered (having stuff soldered is better for my application), then there is less interest in ALC… Any reason why the qwiick module could not be available in ALC?
Some of the confusion may due to the fact that the SparkFun Qwiic Iridium 9603N [product page states: "Need a custom board? This component can be found in SparkFun’s À La Carte board builder… ". Until the Qwiic Iridium is actually available in ALC, it may be a good idea to remove this.