hey…goodafternoon…i hope you all will be fine.i am having a very strange problem, i have 2 wifly RN modules and a pc enabled with wifi card (ITSD).one day i powered up both modules in adhoc mode and run the scan command.first attempt , nothing was found (it should have been found other wifly module and pc with wifly card…) running scan command in module 2, ITSD(wifi card installed in pc) was found.
(why random behaviour)…both modules have been showing random behaviour with scan command…sometimes they found acces points sometimes not, sometimes one module found access points but other didnot…anyone here to help me out plz?? how can i overcome this problem??? thanks
That verion of firmware has a lot of issues with the scan command - update the WiFly to the latest version of firmware.
thanx alot bro for reply… what is the latest version. i think ftp is there for updating versions?? is it ? can you suggest me some commands to look upon for version update…
The WiFly Manual on Roving Networks’ web site lists all of the versions along with details on how to do the update: http://www.rovingnetworks.com/resources … ser_Manual.
thanx Gsm Man. i am trying to update firmware…first i connected to internet through accesspoint(witribe). Connection built successfully…but when i execute "ftp update " command…following things appear
ftp connecting to 208.109.78.34
ftp timeout=2 ![]()
i dont know why this all is happening to me…i have no idea why ftp is timeouting… can anyone help me to get me out of this ?regards
Your command syntax is wrong, you need to supply the file name. Also, you should set the user name, directory and password as they may have changed from the factory default values. Finally, the Roving Networks FTP Servers have moved a couple of times. The full set of commands you should send:
set ftp address 198.175.253.161
set ftp dir ./public
set ftp user roving
set ftp pass Pass123
ftp update wifly7-236.img
great.thanx brother.i ll follow these commands tomorrow in office.i hope they ll work .thankyou
btw how can i confirm that roving networks ftp server address is exactly 198.175.253.161?
Thanks Gsm Man for the working info.
I ever asked Microchip recently how to update fireware because info in the manual did not work.
It took sometime and come back to me with the link to follow. And it did not work either.
Then I sent another ticket saying that I followed your link and did not work and to advise.
I did not receive any reply till now. Maybe they don’t care customer like me because they know that we don’t buy bulk items.
Now I follow Gsm Man info and it works.
Thanks again.
Regards
yeah, GSM man rockx ![]()
Hi,
i have got a wifly (firmeware 2.20). I tried to update it with the commands from gsm man.
The command set ftp dir ./public provokes the “ERR: Bad Args”. I think it is not changeable in that old firmeware version.
The command ftp update wifly7-236.img provokes “FTP timeout=4”
There is a working internet connection (At least i get a response after sending a ping to a server through internet…)
Any ideas?
Thanks!
Hami
Try sending the following and see if you get an error using these commands:
set ftp address 0
set dns name rn.microchip.com
save
ftp update
Thank you for your reply.
i get the following
“FTP connecting to 0.0.0.0”
“FTP timeout=2”
tried that several times…
the command “ping rn.microchip.com” provokes:
“Ping try 198.175.253.161”
and “64 bytes from 198.175.253.161: seq=1 ttl=116 time=254.91 ms”
Tank you for your help
Hami
Solved it. My power supply was too bad.
Hami
hey brother how are you…gosh i need your help. i m also facing “ftp timeout=2” problem.
after sending these commands
set ftp address 0
set dns name rn.microchip.com
ftp update wifly7-236.img
…
i also tried “ftp u”
then i tried these set of commands
{
set ftp address 198.175.253.161
set ftp dir ./public
set ftp user roving
set ftp pass Pass123
ftp update wifly7-236.img
}
but couldnt be able to update the firmware. facing same “ftp timeout=2 error” .you were also facing this problem, i need to know how did you solve it…
i ll be very thankful to you.
regards
The directions on the Roving Networks product support web page worked for me:
RN-131 (version 2.23)
ftp connecting to 208.109.78.34
ftp timeout=2
I am getting this error while trying ftp.Can anyone tell what can i do now?
Did you try the suggestions in the previous posts to this thread?
To upgrade firmware for RN-131 module,i tried few commands
set dns name rn.microchip.com
set ftp address 198.175.253.161
set ftp dir ./public
set ftp user roving
set ftp pass Pass123
ftp update wifly-245.img
time out error 2
ftp update wifly7-245.img
time out error 2
lookup roving1 is also not working.
Can anyone explanin way to resole the matter?
Follow the instructions at Roving Networks: http://www.rovingnetworks.com/FAQs/I_ge … Fly_module
and let us know what happens
I am still getting time out error…
I can not upgrade firmare