I want to use XBee Pro modules in a Digimesh Network with repeat-only nodes to extend the range to more remote sensors. This is solar powered remote and I need absolute minimum power consumption. It is intended to ONLY operate as a repeater in the RF network, and have no local sensors, communications, CPU, etc. connected to any pins. I am using the Sparkfun XBee Breakout board (naked PC Board with only sockets for the XBee pins).
I hoped I could use just +3.3 VDC, Ground, and RST* with a pull-up resistor, with all other pins unconnected. It did not boot even when enclosed in a metal box (no stray ESD). It never appeared in the RF network, was never discovered in the XCTU -based network I had running, no transmissions visible in the spectrum analyzer (FieldFox with RTSA).
These XBees work fine in more complex breakout boards (both proprietary and Sparkfun USB breakouts, including USB based eval boards which use communications pins, etc).
So I added a pull-up resistor to the CONFIG* pin, thinking that may be floating wrong, but still does not boot. Is there some other pin configuration (pull-up or pull down) or power sequencing required? (I cannot find in Digi documentation or Sparkfun forum). Thanks for any info.