tornado  
                
                  
                    September 6, 2010, 10:09pm
                   
                  1 
               
             
            
              Hi,
I have two Xbee Pro 900:
No. 1) Xbee connected to the Xbee Explorer USB and then to my PC
No. 2) Xbee connected to the Xbee Explorer Regulated and then connected to an FTDI chip and then to my PC
I am able to send data from Xbee 1 and then view the data received by Xbee 2.
However if I send data from Xbee 2 the data recieved by Xbee 1 just appears as dots in the terminal program.
I notice that on the Xbee 1 in the terminal program the CTS status is green and on Xbee 2 the CTS is black.
Any idea what is wrong?
Any help would be really appreciated.
Thanks
             
            
              
            
           
          
            
              
                stevech  
              
                  
                    September 6, 2010, 11:08pm
                   
                  2 
               
             
            
              dots mean a baud rate mismatch, I’d guess.
Do both work properly with XCTU’s modem setup tool?
             
            
              
            
           
          
            
              
                tornado  
              
                  
                    September 7, 2010, 12:04am
                   
                  3 
               
             
            
              Both devices have the same baud rate set in the X-CTU program
             
            
              
            
           
          
            
              
                tornado  
              
                  
                    September 7, 2010, 12:06am
                   
                  4 
               
             
            
              The test/query function in X-CTU fails on Xbee 2.
             
            
              
            
           
          
            
              
                tornado  
              
                  
                    September 7, 2010, 12:17am
                   
                  5 
               
             
            
              I think the FTDI board maybe faulty - I will buy a new one and see if that fixes it.
             
            
              
            
           
          
            
              
                beo6  
              
                  
                    October 20, 2010,  8:52am
                   
                  6 
               
             
            
              i think your problem is the diode in the way of the pin for communication.
i am using two Xbee Pro 900 with Xbee Explorer Regulated and had problems like you.
You need to put a wire between the Xbee Din and the Din pin on the Explorer or make a bridge over the diode, but i failed to bridge directly over the diode on the board because of the small form factor.
viewtopic.php?f=13&t=20807 
if you want to see how i did it (it is not nice but it works) i think i can post a picture.