Facet running 3.6
Try to update to 4.2 - facet resets immediately and boots to 3.6
Any suggestions?
configuring both by wifi and terraterm
Facet running 3.6
Try to update to 4.2 - facet resets immediately and boots to 3.6
Any suggestions?
configuring both by wifi and terraterm
Please give the GUI a try.
That did it
Thanks Sparky!
Sparky,
Another question:
If I use external LORA radios, do I need to disable the ESP roadios in both base and Rover?
Glad to hear it!
If I use external LORA radios, do I need to disable the ESP roadios in both base and Rover?
Are you referring to the ESP-NOW radios? They are disabled by default. But to answer your question, yes, disable the ESP-NOW radios if you don’t plan to use them. It’s best to provide only one source of corrections to the GNSS receiver.
If the Base does transmit corrections over external radios and ESP-NOW, the corrections are identical so it shouldn’t cause any problems. We don’t recommend providing the GNSS receiver with multiple different corrections (ie, NTRIP from a service and external radio from a base).
Thanks!
Lee