As describe on the board I apply 5-10V. Exact this rage. It take about 0,12 A, then after some time drops to 0,07. It should be around 0.2A when do nothing and a little more when playing sound
The most basic way to see you your Tsunami is functioning at all is to see if the bootloader will run. Remove any microSD card and plug a 5V USB charger into the USB connector. Press and HOLD the “User” button and then press and release the “Reset” button (keep the “User” button pressed until after you release the “Reset” button.) In a few seconds, the Blue LED should blink slowly. This is the bootloader complaining that there’s no microSD card. If this doesn’t work, then your Tsunami is either defective or has no bootloader.
If this does work, then you can try re-flashing the firmware, although it’s highly unlikely that firmware got corrupted. But inserting a microSD card with the firmware hex file and restarting the bootloader should provide more info about what’s wrong.
Tsunami only supports seamless looping over the length of the file. In other words, the loop start is the first sample frame in the file, and the loop end is the last sample frame in the file.
What I often tell people is that since you can use microSD cards up to 32GB in size, do your looping in a wave editor and make the file the longest that you would ever hold a note.