Is my Olimex LPC-E2294 working?

Hi,

i´ve just got an Olimex LPC-E2294 and i am trying to get started with it.

Should it show any message on the display when powering up?

I tried to get the device id with Philips Flash Utility by using USB (FTDI VCP installed and showing COM4 ready) and also with a serial cable connected between COM1 and the serial connector. None of these worked.

I tried also to upload an HEX file test program via USB cable but without sucess.

Some more information:

With EXT/USB jumper on EXT position, i connect power jack and get power led iluminatting but looks weak. When i connect the USB cable the led iluminates brighter.

With EXT/USB jumper on USB position, i connect USB cable and the power led show two small flashes of light and stays off. The COM4 appears in Windows device manager.

I tried to communicate with the board with JRST and BSL jumpers short and open with the same results.

Did anyone have these problems? Any clues on how to figure out the problem?

Regards.