I just got my Olimex 2294-board from you at Sparkfun. Are you supposed to solder on a power jack yourself? If not, mine’s missing and there is three holes in the board. Also, next to the place where the power jack is supposed to be there’s a D5 missing. Is that also something you have to supply yourself?
davidbinar:
I just got my Olimex 2294-board from you at Sparkfun. Are you supposed to solder on a power jack yourself? If not, mine’s missing and there is three holes in the board. Also, next to the place where the power jack is supposed to be there’s a D5 missing. Is that also something you have to supply yourself?
Best Regards
David Berg
Looks like they forgot to put them on. It’s a bit disturbing, though, as it means that they don’t get tested.
I think they might be tested using the USB-port for power. The board seems to work anyway (The board testing program shows up ok) so I’ll be using the USB-port for power. By the way, do anyone know how to configure the card so I can use the Phillips Flash Utlility. I thought I just had to short the BSL-jumper but the Flash Utility program can’t seem to connect to the card. It just shows: “Cannot communicate with testboard” when I try Read Device ID. (I use 19200 Baud) It works ok with a Bitfire card from Arrow that uses an LPC2129.
I don’t know about the Olimex board, but perhaps you’re specifying a baud rate that is too high. My board has a 12 MHz crystal and I cannot go any higher than 38400 in the flash utility.
PWR jack is not installed on LPC-E2294 intentionally, none of LPC-E2294 have PWR jack (I know I have to replace the first proto picture which is on our web and have PWR jack!)
It was our design flaw that LCD power supply is connected only to USB 5V source (look at the schematic we have on our web), and if the board is powered from the power supply Jack LCD will not light up.
We are working on new revision of the board which will have this fixed
PWR jack is not installed on LPC-E2294 intentionally, none of LPC-E2294 have PWR jack (I know I have to replace the first proto picture which is on our web and have PWR jack!)
It was our design flaw that LCD power supply is connected only to USB 5V source (look at the schematic we have on our web), and if the board is powered from the power supply Jack LCD will not light up.
We are working on new revision of the board which will have this fixed
Ok, thanks for the answer Olimex, I really don’t have a problem with powering the board from USB anyway. Maybe you know something about my perhaps newbie-question about configuring the board to work with the Philips Flash Utility? (I’m using a serial cable from the computer to the card)
By the way, do anyone know how to configure the card so I can use the Phillips Flash Utlility. I thought I just had to short the BSL-jumper but the Flash Utility program can’t seem to connect to the card. It just shows: “Cannot communicate with testboard” when I try Read Device ID. (I use 19200 Baud) It works ok with a Bitfire card from Arrow that uses an LPC2129.