I have purchased the MSP430-JTAG-TINY, and I am trying to use it with the TI code-composer-studio-4 IDE but can’t find any instructions for installation.
In Sparkfun’s product page it is written that “MSP430.dll makes it compatible with all existing software which works with TI-USB-FET (emulates TI-USB-FET)”, so I was installing the driver, replaced the MSP430.dll and added the rest of olimex’s .dll files into Program Files\Texas Instruments\ccs4\ccsv4\DebugServer\drivers, but can’t configure ccs4 to work with the debugger because it won’t show the “Olimex” option int the debugger list.
Im using Code Composer 4 and Olimex MSP430-JTAG-TINY-V2. I have followed the instructions on the Olimex Homepage to get the Programmer running with CC4 (copying .dll …). When I try to start a debug session I always get an error, that a new firmaware for programmer is needed. And if I click onto update button the tool tries to update and after this it ask again for update. I also updated my Programmer using the Olimex programming tool with the newest Firmware (1.04) but it does not help. Has any body experiences with the version 2 debugger? Some colleagues using version 1 without any problems.
Reconfigure the target config (if necessary) to use the “TI MSP430 USB1 (Default)”. I renamed the MSP430.DLL that was there to MSP$430.DLL.OLD, just in case.