Hello, all.
I want to update my Facet’s firmware to the latest, v3.3, I believe. With all of the online help information found, and after searching this forum, I am still floundering and hope someone can set me straight.
I found the firmware update instructions which say, with this v1.10 firmware one must use the “Updating Firmware Using The Uploader GUI” method. I downloaded the RTK Firmware Uploader v1.5.2 to my Mac. The Mac is running Ventura 13.3.1(a). I downloaded the file RTK_Surveyor_Firmware_v3_3.bin from the github repository.
The Facet is plugged into the Mac via a USB cable, turned on, and in Rover mode. In the RTK Firmware Loader, the only COM ports that appear in the drop-down menu are:
(cu.BLTH)
(tty.BLTH)
(cu.Bluetooth-Incoming-Port)
(tty.Bluetooth-Incoming-Port)
There are none that hint at using a USB port.
In the Firmware Uploader instructions, there is this line: “On Windows, open the Device Manager to confirm which COM port the device is operating on. On other platforms, check /dev.”
I looked through /dev directory and didn’t see anything obvious. No new devices appear in the directory after plugging the Facet into the USB port and turning it on.
Three baud rate choices are in the drop-down menu, though I have no clue which, if any, is correct.
When clicking on the Upload Firmware button on Firmware Uploader, the status/warnings goes through the motions, but definitely does not update the firmware.
I hope someone can please help! Thank you very much.
Regards,
-Gary