rejected by the DRC bot

The DRC bot failed my board for violating the 8 mil trace width limit. My traces are all greater than 8 mils and the only thing highlighted in the picture I got in the email is a single pixel vertical line down the right edge of the board:

http://img5.imageshack.us/img5/2981/topig.png

any ideas? There certainly arent any components or traces over there… The edge of the polygon is there but I tried moving it away and re uploading but it still failed.

Also definitely no errors on the bottom layer.

edit: heres the log for the top layer:

unmatched 274X paramblock OFA0B0 - len 6
Macro Name = OC8
Macro Consuming 5,1,8,0,0,1.08239X$1,22.5 [2]
PUSH 1.000000
PUSH 8.000000
PUSH 0.000000
PUSH 0.000000
PUSH 1.082390
FETCH 1
MUL
PUSH 22.500000
PRIM 5
Parse_OK
Arg: 0.0600
Looking up macro OC8 [0x671160]
Beginning GCODE run
Ending GCODE run
Created 6397 polygons
Found 0 errors
Partitioning....
Grouping...
Distance testing
MergeCount: 6234
tests: 2075295
Board boundaries: Rect: [0.018100,0.021100] -> [2.774100,2.777100], w: 2.756000, h: 2.756000
Found 163 groups
lengthdb size 0
DRC space fail: [0x780870 0x783750] 0.000100 - 0.006900
DRC space fail: [0x780870 0x7915d0] 0.000100 - 0.006900
DRC space fail: [0x783750 0x780870] 0.000100 - 0.006900
DRC space fail: [0x784b50 0x784bf0] 0.000100 - 0.006900
DRC space fail: [0x784bf0 0x784b50] 0.000100 - 0.006900
DRC space fail: [0x784bf0 0x788ed0] 0.000100 - 0.006900
DRC space fail: [0x788ed0 0x784bf0] 0.000100 - 0.006900
DRC space fail: [0x7915d0 0x780870] 0.000100 - 0.006900

Hmm, looks like a bot bug. Send an email to the batchpcb guys + they probably will clear the design manually.

–David Carne

What are the circles with the really fine lines in the mounting holes (and 2 other holes)? I’ve never used BatchPCB before, but I bet they don’t let you define holes like that. Why didn’t you just put these in the drill file with the other holes?

They’re holes made using the Hole command in eagle. The fine line circle is the dimension layer, just like the fine line around perimeter.

edit: but to avoid future problems Ill likely take that advice

Those holes are still in the drill file as well - some CAM jobs just add it to the gerber output. They won’t cause any problems.

–David Carne