SPX-17369 SparkFun RTK Surveyor
Order number: 6499673
Order date: Saturday, February 20, 2021
Received: 2/26/2021, first used ~ 12 March
At first things went quite well. I am using a Lenovo Tab M10 FHD Plus
wih Android 10 to run the latest SW Maps.
SW Maps communicated via BlueTooth with the RTK Surveyor and the data was
wonderful (and SW Maps too).
But today (Sunday) it suddenly ceased pairing - it was OK before lunch,
but dead when I came back to it.
The blue pair light blinks, but does not connect. When I try to
connect, either via SW Maps or Android’s “Connected Devices”, an
error is reported.
I checked with a desktop Mac and an iPad and neither shows the RTK in
the list of discoverable BlueTooth devices (I know it won’t work with
an Apple computer, but it should show it as a possible BlueTooth device)
The yellow PPS light blinks, suggesting that the u-blox is still
functioning and receiving satellites.
The SparkFun forum #223233 suggested checking inside that both switches
are up, so I checked checked & cycled the switches in case they were
making a poor connection. No change…
Battery is fully charged.
I searched the Forum extensively, but could not find any postings
relevant to my issue.
So, I am at a loss as to what the next trouble-shooting step should be.
Since the u-blox appears to be working, iI suspect the ESP32 WROOM , which
appears to be in charge of BT communications, may have bit the dust…
Help!
Cordially,
–
Garth Fletcher