STHS34PF80 Presence and motion sensor module not working

In my case, the module connections are accurate, and the sensor is detecting output correctly up to two feet’s, after that, there’s no detection or functioning properly—what could be the causes? Module coverage issue not identified according to datasheet specifications. I am using ESP32 module.

Many modules meet “datasheet range” only at their rated VDD. Measure VDD at the module while ranging far targets.The device power supply must be provided through the VDD line, a power supply decoupling capacitor (100 nF) must be placed as near as possible to the supply pins of device (VDD). Depending on the application, an additional capacitor of 1 µF could be placed on the VDD line to avoid power noise on VDD.

If you wanna switch to a simpler motion sensor, you can consider RCWL-0516 All About RCWL-0516 Microwave Radar Motion Sensor - Share Project - PCBWay

1 Like

okay mam thank you i check it out

Input voltage to the module I checked it there is no dip or deviations and no noise there still I am not getting expected coverage. What could be other reasons?