Tsunami firmware upgrade question

Hi,

I tried upgrading my tsunami to the latest mono firmware version:

https://robertsonics.com/resources/tsun … _v109m.zip

It seemed to work but was i wasnt 100% sure if it did as the upgrade was incredibly fast.

So, today i tried to do it again with the same version. This time, i get the error : long solid, 2 short flashes, which is an issue with the hex file. Imtried copying it multiple times…

My question is: does this seem like an issue? Or, should i expect this error if i try and upload t

Version of the firmware over the top of itself?

Thanks

The firmware update is indeed very fast.

There’s no reason you can’t update with the same version you’re already running. Did you try downloading a new copy of the firmware hex file?

Hi, ok, i got it working. I had a capital T in the filename. Sorry my bad!

This module is amazing. Ive got it running in my modular. So cool. Thanks for the amazing work!!!